Home > MPC Configurator

Swagelok Modular Platform Components (MPC) Configurator

MPC Configurator

The MPC Configurator is an interactive tool to build and assemble ANSI/ISA 76.00.02-compliant miniature modular designs prior to the purchase process.

To download and install the Swagelok MPC Configurator:

  1. Please select the version of the MPC Configurator that you would like to download by clicking this link for the 32-bit version: Swagelok MPC Configurator 1.7 - 32-bit or this link for the 64-bit version: Swagelok MPC Configurator 1.7 - 64-bit.
    • The program file is 97 MB.
    • The configurator is in English.
    • The program is a self extracting zip file. Winzip in not needed for the install.
  2. Double click the MPC Configurator Installation file. The install process will begin.
  3. At the MPC Welcome screen, select "Next."
  4. At the License Agreement screen, you will need to Agree to the license agreement and select “Next” to continue.
  5. The installation process will put the MPC configurator files in a folder called "C:\Program Files\Swagelok\MPC Configurator 1.7". If you want to use the default folder, then click the “Next” button. If you want to put the files in a different folder, click "Browse" button and select another folder. When finished, click the “Next” button to proceed.
  6. Click “Next” to start the install.
  7. The files are copied and registered on your computer. The next screen indicates Swagelok MPC setup was completed successfully. Select “Close” to complete the process.

Read the Frequently Asked Questions for the MPC Configurator.

System Requirements:
The configurator is in English only at this time.
The zip file is 97 MB.
150 MB hard disk space needed.
Microsoft Windows XP, Microsoft Windows Vista (any version), or Microsoft Windows 7 (any version)
.NET 3.5.1 Framework
CAD Output Requirements: AutoCAD 2010 and SolidWorks 2007, 2008, 2009, or 2010

Einloggen oder jetzt anmelden
Melden Sie sich an, um Preise abzurufen, Angebote anzufordern und online zu bestellen.
 

Wir helfen Ihnen seit über 60 Jahren.


Fluidsystemschulungen, damit Sie schneller produktiv werden.